H+S
For more than 30 years, H+S has been supplying precision foils and sheets of high-specification carbon steel, stainless steels and non-ferrous metals (such as copper, brass, bronze, nickel, and aluminium).
The product range of H+S is the culmination of practical experience in the field, adapted to the market demands dictated by diverse clients across the broad array of industries in which H+S is active. Laser-cut pieces can be produced from foil strips of various materials, at the request of the client and according to client specifications.
700 products available in stock
The metal foils have a precise thickness tolerance (T3). The following thicknesses can all be supplied:
700 products available in stock
The metal foils have a precise thickness tolerance (T3). The following thicknesses can all be supplied:
- Up to 0.06 mm (in increments of 0.005 mm)
- Up to 0.30 mm (in increments of 0.01 mm)
- Up to 1.00 mm (in increments of 0.05 mm)
- Up to 2.00 mm (in increments of 0.10 mm)
- Up to 3.20 mm (in increments of 0.20 mm)
- Plus, 3.54 - 3.80 - 4.00 and 5.03 mm